DmBndBuilderUsePartTypes Enumeration

NXOpen.CAM.DmBndBuilder.UsePartTypes is an alias for NXOpen.CAM.DmBndBuilderUsePartTypes

class NXOpen.CAM.DmBndBuilderUsePartTypes

Bases: object

Available types for boundary use part cantainment Option

Enum Members

Enum Member Enum Member Description
PartContainOff
Part Containment Off
PartContainLargestLoop
Part Containment Largest Loop
PartContainAllLoops
Part Containment All Loops
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.