DmBndBuilderBndPatternCenterTypes Enumeration

NXOpen.CAM.DmBndBuilder.BndPatternCenterTypes is an alias for NXOpen.CAM.DmBndBuilderBndPatternCenterTypes

class NXOpen.CAM.DmBndBuilderBndPatternCenterTypes

Bases: object

Available types for Boundary Pattern Center in FASurfaceContour

Enum Members

Enum Member Enum Member Description
MethodAutomatic
Automatic
MethodSpecify
Specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.