DmAmBuilderAutoPatCenterTypes Enumeration

NXOpen.CAM.DmAmBuilder.AutoPatCenterTypes is an alias for NXOpen.CAM.DmAmBuilderAutoPatCenterTypes

class NXOpen.CAM.DmAmBuilderAutoPatCenterTypes

Bases: object

Available types for area milling Auto Pattern Center

Enum Members

Enum Member Enum Member Description
Automatic
Automatic
Specify
Specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.