DmAmBuilderAmCutPatternTypes Enumeration

NXOpen.CAM.DmAmBuilder.AmCutPatternTypes is an alias for NXOpen.CAM.DmAmBuilderAmCutPatternTypes

class NXOpen.CAM.DmAmBuilderAmCutPatternTypes

Bases: object

Available types for Area Milling cut pattern in FASurfaceContour

Enum Members

Enum Member Enum Member Description
FollowPeriphery
Follow Periphery
Profile
Profile
Sep1
separate one
ParallelLines
Parallel Lines
RadialLines
Radial Lines
ConcArcs
Concentric Arcs
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.