DmAmBuilderAmCustomStartTypes Enumeration

NXOpen.CAM.DmAmBuilder.AmCustomStartTypes is an alias for NXOpen.CAM.DmAmBuilderAmCustomStartTypes

class NXOpen.CAM.DmAmBuilderAmCustomStartTypes

Bases: object

Available types for in FASurfaceContour

Enum Members

Enum Member Enum Member Description
Custom
Area Milling Custom Start Custom
Automatic
Area Milling Custom Start Automatic
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.