DisplayPathPathDisplayTypes Enumeration

NXOpen.CAM.DisplayPath.PathDisplayTypes is an alias for NXOpen.CAM.DisplayPathPathDisplayTypes

class NXOpen.CAM.DisplayPathPathDisplayTypes

Bases: object

the path display types

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
SolidCenter
Path Display: Solid Center
DashedCenter
Path Display: Dashed Center
Silhouette
Path Display: Silhouette
Fill
Path Display: Fill
SilhouetteFill
Path Display: Silhouette Fill
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.