DPMItpBuilderStepoverTypeOption Enumeration

NXOpen.CAM.DPMItpBuilder.StepoverTypeOption is an alias for NXOpen.CAM.DPMItpBuilderStepoverTypeOption

class NXOpen.CAM.DPMItpBuilderStepoverTypeOption

Bases: object

Enum of stepover type

Enum Members

Enum Member Enum Member Description
Number
stepover number
Distance
stepover distance
Scallop
stepover scallop height
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.