CycleTipRelease Class¶
-
class
NXOpen.CAM.
CycleTipRelease
¶ Bases:
NXOpen.TaggedObject
Represets a User Defined Event
New in version NX10.0.2.
Properties¶
Property | Description |
---|---|
Distance | Returns or sets the coolant mode |
IsActive | Returns or sets the tip release status |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
Distance¶
-
CycleTipRelease.
Distance
¶ Returns or sets the coolant mode
-------------------------------------
Getter Method
Signature
Distance()
Returns: the tip release distance Return type: float New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Distance(tipRelease)
Parameters: tipRelease (float) – the tip release distance New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
IsActive¶
-
CycleTipRelease.
IsActive
¶ Returns or sets the tip release status
-------------------------------------
Getter Method
Signature
IsActive()
Returns: the tip release mode status Return type: bool New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsActive(bActive)
Parameters: bActive (bool) – the tip release mode status New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)