CycleStepRetract Class¶
-
class
NXOpen.CAM.
CycleStepRetract
¶ Bases:
NXOpen.TaggedObject
Represets a User Defined Event
New in version NX10.0.2.
Properties¶
Property | Description |
---|---|
IsActive | Returns or sets the Step Retract status |
RetractValue | Returns or sets the step retract value |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
IsActive¶
-
CycleStepRetract.
IsActive
¶ Returns or sets the Step Retract status
-------------------------------------
Getter Method
Signature
IsActive()
Returns: the Step Retract active status Return type: bool New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
IsActive(bActive)
Parameters: bActive (bool) – the Step Retract active status New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
RetractValue¶
-
CycleStepRetract.
RetractValue
¶ Returns or sets the step retract value
-------------------------------------
Getter Method
Signature
RetractValue()
Returns: the StepRetractvalue Return type: float New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
RetractValue(doubleValue)
Parameters: doubleValue (float) – the step retract value New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)