CycleNodragClearance Class¶
-
class
NXOpen.CAM.
CycleNodragClearance
¶ Bases:
NXOpen.TaggedObject
Represets a User Defined Event
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
IsActive | Returns or sets the Nodrag Clearance status |
NodragValue | Returns or sets the Nodrag Clearance value |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
IsActive¶
-
CycleNodragClearance.
IsActive
¶ Returns or sets the Nodrag Clearance status
-------------------------------------
Getter Method
Signature
IsActive()
Returns: the Nodrag Clearance active status Return type: bool New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
IsActive(bActive)
Parameters: bActive (bool) – the Nodrag Clearance active status New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
NodragValue¶
-
CycleNodragClearance.
NodragValue
¶ Returns or sets the Nodrag Clearance value
-------------------------------------
Getter Method
Signature
NodragValue()
Returns: the NodragClearancevalue Return type: float New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
NodragValue(doubleValue)
Parameters: doubleValue (float) – the Nodrag Clearance value New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)