CycleDwellType Enumeration

NXOpen.CAM.Cycle.DwellType is an alias for NXOpen.CAM.CycleDwellType

class NXOpen.CAM.CycleDwellType

Bases: object

Available types for dwell

Enum Members

Enum Member Enum Member Description
On
dwell on
Off
dwell off
Seconds
dwell seconds
Revolutions
dwell revolutions
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.