CycleDwell Class¶
-
class
NXOpen.CAM.
CycleDwell
¶ Bases:
NXOpen.TaggedObject
Represets a User Defined Event
New in version NX10.0.2.
Properties¶
Property | Description |
---|---|
Dwell | Returns or sets the dwell value |
DwellMode | Returns or sets the dwell type |
IsActive | Returns or sets the dwell status |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
CycleDwellMode Enumeration | Available types for dwell mode |
Property Detail¶
Dwell¶
-
CycleDwell.
Dwell
¶ Returns or sets the dwell value
-------------------------------------
Getter Method
Signature
Dwell()
Returns: the dwell value Return type: float New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Dwell(doubleValue)
Parameters: doubleValue (float) – the dwell value New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
DwellMode¶
-
CycleDwell.
DwellMode
¶ Returns or sets the dwell type
-------------------------------------
Getter Method
Signature
DwellMode()
Returns: the dwell mode Return type: NXOpen.CAM.CycleDwellMode
New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
DwellMode(dwell)
Parameters: dwell ( NXOpen.CAM.CycleDwellMode
) – the dwell modeNew in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
IsActive¶
-
CycleDwell.
IsActive
¶ Returns or sets the dwell status
-------------------------------------
Getter Method
Signature
IsActive()
Returns: the dwell mode status Return type: bool New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
IsActive(bActive)
Parameters: bActive (bool) – the dwell mode status New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)