CutterExportTrackpointExportStatus Enumeration¶
NXOpen.CAM.CutterExport.TrackpointExportStatus is an alias for NXOpen.CAM.CutterExportTrackpointExportStatus
-
class
NXOpen.CAM.
CutterExportTrackpointExportStatus
¶ Bases:
object
the trackpoint export status
Enum Members
Enum Member Enum Member Description Ok Trackpoint has been export successfullyUnchanged Trackpoint in library unchangedUndefined Trackpoint is not definedUntried Trackpoint export didn’t happenFail Trackpoint export failed-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-