CutterExportHolderExportStatus Enumeration¶
NXOpen.CAM.CutterExport.HolderExportStatus is an alias for NXOpen.CAM.CutterExportHolderExportStatus
-
class
NXOpen.CAM.
CutterExportHolderExportStatus
¶ Bases:
object
the holder export status
Enum Members
Enum Member Enum Member Description Ok Holder has been export successfullyUnchanged Holder in library unchangedUndefined Holder is not definedUntried Holder export didn’t happenFail Holder export failed-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-