Cutcom Class

class NXOpen.CAM.Cutcom

Bases: NXOpen.TaggedObject

Represents a NXOpen.CAM.Cutcom

New in version NX6.0.2.

Properties

Property Description
MinimumAngle Returns or sets the cutter compensation minimum angle
MinimumMove Returns the cutter compensation minimum move builder (inheritable tool dep)
OutputContactPoint Returns or sets the cutter compensation output contact point status
OutputPlane Returns or sets the cutter compensation output plane status
Suppress Returns or sets the suppress cutter compensation
Tag Returns the Tag for this object.
TrackingPointType Returns or sets the cutter compensation tracking point selection
Type Returns or sets the cutter compensation type

Methods

Enumerations

CutcomTypes Enumeration Available types for cutter compensation in planar milling

Property Detail

MinimumAngle

Cutcom.MinimumAngle

Returns or sets the cutter compensation minimum angle

-------------------------------------

Getter Method

Signature MinimumAngle()

Returns:
Return type:float

New in version NX6.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature MinimumAngle(minimumAngle)

Parameters:minimumAngle (float) –

New in version NX6.0.2.

License requirements: cam_base (“CAM BASE”)

MinimumMove

Cutcom.MinimumMove

Returns the cutter compensation minimum move builder (inheritable tool dep)

-------------------------------------

Getter Method

Signature MinimumMove()

Returns:The cutcom minimum move builder
Return type:NXOpen.CAM.InheritableToolDepBuilder

New in version NX6.0.2.

License requirements: None.

OutputContactPoint

Cutcom.OutputContactPoint

Returns or sets the cutter compensation output contact point status

-------------------------------------

Getter Method

Signature OutputContactPoint()

Returns:
Return type:bool

New in version NX6.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature OutputContactPoint(newValue)

Parameters:newValue (bool) –

New in version NX6.0.2.

License requirements: cam_base (“CAM BASE”)

OutputPlane

Cutcom.OutputPlane

Returns or sets the cutter compensation output plane status

-------------------------------------

Getter Method

Signature OutputPlane()

Returns:
Return type:bool

New in version NX6.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature OutputPlane(outputPlane)

Parameters:outputPlane (bool) –

New in version NX6.0.2.

License requirements: cam_base (“CAM BASE”)

Suppress

Cutcom.Suppress

Returns or sets the suppress cutter compensation

-------------------------------------

Getter Method

Signature Suppress()

Returns:
Return type:bool

New in version NX6.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature Suppress(suppress)

Parameters:suppress (bool) –

New in version NX6.0.2.

License requirements: cam_base (“CAM BASE”)

TrackingPointType

Cutcom.TrackingPointType

Returns or sets the cutter compensation tracking point selection

-------------------------------------

Getter Method

Signature TrackingPointType()

Returns:
Return type:int

New in version NX6.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature TrackingPointType(newValue)

Parameters:newValue (int) –

New in version NX6.0.2.

License requirements: cam_base (“CAM BASE”)

Type

Cutcom.Type

Returns or sets the cutter compensation type

-------------------------------------

Getter Method

Signature Type()

Returns:
Return type:NXOpen.CAM.CutcomTypes

New in version NX6.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(type)

Parameters:type (NXOpen.CAM.CutcomTypes) –

New in version NX6.0.2.

License requirements: cam_base (“CAM BASE”)