CutStrategyTypes Enumeration¶
NXOpen.CAM.CutStrategy.Types is an alias for NXOpen.CAM.CutStrategyTypes
-
class
NXOpen.CAM.
CutStrategyTypes
¶ Bases:
object
The cut strategy options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description LevelZ Cut strategy: Level ZigLevelZz Cut strategy: Level Zig-ZagRampingZ Cut strategy: Ramping ZigRampingZz Cut strategy: Ramping Zig-ZagContourZ Cut strategy: Contour ZigContourZz Cut strategy: Ramping Zig-ZagPlungeZ Cut strategy: Plunge ZigPlungeZz Cut strategy: Plunge Zig-ZagPlungeAlt Cut strategy: Plunge AlternatePlungeCastleing Cut strategy: Plunge CastleingPartOff Cut strategy: Part OffBlankContourZ Cut strategy: Blank Contour Zig-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-