CutParametersCutConnectionTypes Enumeration

class NXOpen.CAM.CutParametersCutConnectionTypes

Bases: object

Available types for cut connection

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
Traverse
Cut connection: Traverse
ContinuousCuts
Cut connection: Continuous Cuts
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.