CutLevelRangeTypes Enumeration

NXOpen.CAM.CutLevel.RangeTypes is an alias for NXOpen.CAM.CutLevelRangeTypes

class NXOpen.CAM.CutLevelRangeTypes

Bases: object

range types

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Automatic
Automatic
UserDefined
User Defined
Single
Single
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.