CutLevelMeasureTypes Enumeration

NXOpen.CAM.CutLevel.MeasureTypes is an alias for NXOpen.CAM.CutLevelMeasureTypes

class NXOpen.CAM.CutLevelMeasureTypes

Bases: object

measure from types

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
TopLevel
Top Level
RangeTop
Current Range Top
RangeBottom
Current Range Bottom
WcsOrigin
WCS Origin
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.