CutDwell Class¶
-
class
NXOpen.CAM.
CutDwell
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.CutDwell
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Revolutions | Returns or sets the cut dwell revolutions |
Tag | Returns the Tag for this object. |
Time | Returns or sets the cut dwell time |
Type | Returns or sets the cut dwell type |
Methods¶
Enumerations¶
CutDwellTypes Enumeration | the rough cut dwell mode options |
Property Detail¶
Revolutions¶
-
CutDwell.
Revolutions
¶ Returns or sets the cut dwell revolutions
-------------------------------------
Getter Method
Signature
Revolutions()
Returns: the cut dwell revolutions Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Revolutions(cutDwellRevolutionsValue)
Parameters: cutDwellRevolutionsValue (float) – the cut dwell revolutions New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Time¶
-
CutDwell.
Time
¶ Returns or sets the cut dwell time
-------------------------------------
Getter Method
Signature
Time()
Returns: the cut dwell time Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Time(cutDwellTimeValue)
Parameters: cutDwellTimeValue (float) – the cut dwell time New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Type¶
-
CutDwell.
Type
¶ Returns or sets the cut dwell type
-------------------------------------
Getter Method
Signature
Type()
Returns: the cut dwell type Return type: NXOpen.CAM.CutDwellTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(cutDwellValue)
Parameters: cutDwellValue ( NXOpen.CAM.CutDwellTypes
) – the cut dwell typeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)