CutDirectionTypes Enumeration

NXOpen.CAM.CutDirection.Types is an alias for NXOpen.CAM.CutDirectionTypes

class NXOpen.CAM.CutDirectionTypes

Bases: object

Available types for cut direction type in boundary cut direction customizable item

Enum Members

Enum Member Enum Member Description
Climb
Climb Cut
Conventional
Conventional Cut
Forward
Follow Boundary
Reverse
Reverse Boundary
Mixed
Mixed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.