CornerControlBuilderSmoothCornersAtOptions Enumeration

NXOpen.CAM.CornerControlBuilder.SmoothCornersAtOptions is an alias for NXOpen.CAM.CornerControlBuilderSmoothCornersAtOptions

class NXOpen.CAM.CornerControlBuilderSmoothCornersAtOptions

Bases: object

Available options where Corner Smoothing should be applied

Enum Members

Enum Member Enum Member Description
Boundary
Boundary
PartSurface
Part Surface
BoundaryAndPartSurface
Boundary and Part Surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.