CornerControlBuilderCornerControlMethods Enumeration

NXOpen.CAM.CornerControlBuilder.CornerControlMethods is an alias for NXOpen.CAM.CornerControlBuilderCornerControlMethods

class NXOpen.CAM.CornerControlBuilderCornerControlMethods

Bases: object

Available methods for Corner Control

Enum Members

Enum Member Enum Member Description
RollAround
Roll Around
ExtendAndTrim
Extend and Trim
Extend
Extend
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.