ContourAngle Class¶
-
class
NXOpen.CAM.
ContourAngle
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.ContourAngle
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Maximum | Returns or sets the maximum face angle |
Minimum | Returns or sets the minimum face angle |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
Maximum¶
-
ContourAngle.
Maximum
¶ Returns or sets the maximum face angle
-------------------------------------
Getter Method
Signature
Maximum()
Returns: the maximum face angle Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Maximum(maxAngle)
Parameters: maxAngle (float) – the maximum face angle New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Minimum¶
-
ContourAngle.
Minimum
¶ Returns or sets the minimum face angle
-------------------------------------
Getter Method
Signature
Minimum()
Returns: the minimum face angle Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Minimum(minAngle)
Parameters: minAngle (float) – the minimum face angle New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)