CircularAboutAxisMoveBuilderAxisType Enumeration

NXOpen.CAM.CircularAboutAxisMoveBuilder.AxisType is an alias for NXOpen.CAM.CircularAboutAxisMoveBuilderAxisType

class NXOpen.CAM.CircularAboutAxisMoveBuilderAxisType

Bases: object

the axis type

Enum Members

Enum Member Enum Member Description
Tool
Tool Axis
Vector
Vector
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.