ChamferMillingBuilderChamferReferenceType Enumeration¶
NXOpen.CAM.ChamferMillingBuilder.ChamferReferenceType is an alias for NXOpen.CAM.ChamferMillingBuilderChamferReferenceType
-
class
NXOpen.CAM.
ChamferMillingBuilderChamferReferenceType
¶ Bases:
object
Available types for chamfer reference
Enum Members
Enum Member Enum Member Description MaxDiameter reference to max (C-Sink) diameterMinDiameter reference to min (Hole) diameter-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-