CenterlineDrillTurningBuilderCycleTypes Enumeration

NXOpen.CAM.CenterlineDrillTurningBuilder.CycleTypes is an alias for NXOpen.CAM.CenterlineDrillTurningBuilderCycleTypes

class NXOpen.CAM.CenterlineDrillTurningBuilderCycleTypes

Bases: object

the centerline cycle types

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
Drill
Cycle: Drill
DrillDeep
Cycle: Drill, Deep
DrillBreakChip
Cycle: Drill, Break Chip
Tap
Cycle: Tap
TapFloat
Cycle: Tap, Float
Bore
Cycle: Bore
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.