CamOperationMotionContactDataType Struct¶
-
class
NXOpen.CAM.
CamOperationMotionContactDataType
¶ Bases:
object
Motion contact data type .
Constructor: NXOpen.CAM.CamOperationMotionContactDataType()
Fields¶
Field | Description |
---|---|
ContactPt | If motion is contact, this is the contact position. |
ContactArcAxis | |
ContactArcCenter | Contact arc center |
ContactArcRadius | Contact arc radius |
ContactShape |
ContactPt¶
-
CamOperationMotionContactDataType.
ContactPt
¶ If motion is contact, this is the contact position.
-------------------------------------
Field Value Type:
NXOpen.CAM.CamOperationMotionPosType
ContactArcAxis¶
-
CamOperationMotionContactDataType.
ContactArcAxis
¶ -------------------------------------
Field Value Type:
NXOpen.Vector3d
ContactArcCenter¶
-
CamOperationMotionContactDataType.
ContactArcCenter
¶ Contact arc center
-------------------------------------
Field Value Type:
NXOpen.Point3d
ContactArcRadius¶
-
CamOperationMotionContactDataType.
ContactArcRadius
¶ Contact arc radius
-------------------------------------
Field Value Type:float
ContactShape¶
-
CamOperationMotionContactDataType.
ContactShape
¶ -------------------------------------
Field Value Type:
NXOpen.CAM.CamOperationMotionShapeType