CamInspectionOperationFeaturetypes Enumeration¶
-
class
NXOpen.CAM.
CamInspectionOperationFeaturetypes
¶ Bases:
object
Specifies the type of an inspection feature Enum Members
Enum Member Enum Member Description NotSet Not a FeatureArc ArcCircle CirclePoint PointSphere SphereSurface SurfacePattern PatternCurve CurveCylinder CylinderCone ConePlane PlaneLine LineCparln Closed Parallel Line bounded slotSlotTab Slot or TabSurfaceOfRevolution Surface of RevolutionTorus Torus-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-