CAMSetupPostprocessSettingsReviewTool Enumeration¶
NXOpen.CAM.CAMSetup.PostprocessSettingsReviewTool is an alias for NXOpen.CAM.CAMSetupPostprocessSettingsReviewTool
-
class
NXOpen.CAM.
CAMSetupPostprocessSettingsReviewTool
¶ Bases:
object
Review tool setting for Postprocess
Enum Members
Enum Member Enum Member Description On show the review tool windowOff not show the review tool windowPostDefined use post defined setting-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-