CAMSessionObjectSubtype Enumeration

NXOpen.CAM.CAMSession.ObjectSubtype is an alias for NXOpen.CAM.CAMSessionObjectSubtype

class NXOpen.CAM.CAMSessionObjectSubtype

Bases: object

the template subtype class

Enum Members

Enum Member Enum Member Description
Setup
Setup
Operation
Operations
Program
NC Program
Tool
Machine Tools and Cutters
Method
Machining Method
Geometry
Geometry
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.