CAMObjectStatus Enumeration¶
NXOpen.CAM.CAMObject.Status is an alias for NXOpen.CAM.CAMObjectStatus
-
class
NXOpen.CAM.
CAMObjectStatus
¶ Bases:
object
The status of the object
Enum Members
Enum Member Enum Member Description Complete Object path has been outputRepost Object path must be post-processedRegen Object path must be regeneratedApproved Object path has been approved as is-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-