CAMObjectAttr Enumeration¶
NXOpen.CAM.CAMObject.Attr is an alias for NXOpen.CAM.CAMObjectAttr
-
class
NXOpen.CAM.
CAMObjectAttr
¶ Bases:
object
Represents the CAM attribute type.
Enum Members
Enum Member Enum Member Description ProjDiffTaxis ProfileFlipMside BndSplineTangent BlankNormalDiffTaxis BndHasSleepObj ClrnrNotParallelTaxis BndNotParallelFloor FloorNotUpToDate SingleProfileWithFirstCut CutterConversionProblem AcceptDrivePosition Reparametrization BetweenFromStart CurveCutRange FixGssmCornerData PlmConversion PlmFeedcomp PlmFillet PlmSlowdown PlmGeometry WedmPoints CavityMillInheritTrimBnds RtdObsolete ZlevelHolderParamChange NcmObsoleteSeqControl NcmObsoleteCustomFeed NcmObsoleteLocalRetract NcmClearTraversalZero NcmObsoleteEngretToClearance GmcInvalidNxVersion ProbingInvalidNxVersion InspPathInvalidNxVersion CustomDataGougingObsolete CustomDataGougingPartObsolete CustomDataGougingDriveObsolete CustomDataIgnoreLoopsObsolete CustomDataIgnoreLoopsRemoved LimitToolRunOn -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-