CAMFeatureState Enumeration¶
NXOpen.CAM.CAMFeature.State is an alias for NXOpen.CAM.CAMFeatureState
-
class
NXOpen.CAM.
CAMFeatureState
¶ Bases:
object
Update status of the feature
Enum Members
Enum Member Enum Member Description Deleted Feature is not validChanged Feature is changed and out of dateUpdated Feature is changed and updatedUpToDate Feature is up to date-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-