CAMFeatureProcessStatus Enumeration¶
NXOpen.CAM.CAMFeature.ProcessStatus is an alias for NXOpen.CAM.CAMFeatureProcessStatus
-
class
NXOpen.CAM.
CAMFeatureProcessStatus
¶ Bases:
object
Process status of the feature
Enum Members
Enum Member Enum Member Description Empty Feature has no operationsRegenerate One or more of the feature’s operation toolpaths need to regenerateIncomplete One or more of the feature’s operation toolpaths are not completedComplete The feature’s operation toolpaths are complete-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-