BoundaryTurnVariableStockSet Class¶
-
class
NXOpen.CAM.
BoundaryTurnVariableStockSet
¶ Bases:
NXOpen.TaggedObject
Represents a turning boundary variable stock set
To create a new instance of this class, use
NXOpen.CAM.BoundaryTurnVariableStock.CreateItemBuilder()
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
DistanceFromBoundary | Returns or sets the distance from boundary |
Feed | Returns or sets the feed rate toggle |
FeedUnit | Returns or sets the feed rate unit |
FeedValue | Returns or sets the feed rate value |
PositionFromStart | Returns or sets the position from start |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
BoundaryTurnVariableStockSetFeedType Enumeration | the feed rate types available |
Property Detail¶
DistanceFromBoundary¶
-
BoundaryTurnVariableStockSet.
DistanceFromBoundary
¶ Returns or sets the distance from boundary
-------------------------------------
Getter Method
Signature
DistanceFromBoundary()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceFromBoundary(distFromBoundary)
Parameters: distFromBoundary (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Feed¶
-
BoundaryTurnVariableStockSet.
Feed
¶ Returns or sets the feed rate toggle
-------------------------------------
Getter Method
Signature
Feed()
Returns: Return type: NXOpen.CAM.BoundaryTurnVariableStockSetFeedType
New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
Feed(newValue)
Parameters: newValue ( NXOpen.CAM.BoundaryTurnVariableStockSetFeedType
) –New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
FeedUnit¶
-
BoundaryTurnVariableStockSet.
FeedUnit
¶ Returns or sets the feed rate unit
-------------------------------------
Getter Method
Signature
FeedUnit()
Returns: Return type: NXOpen.CAM.BoundaryTurnSetFeedUnitTypes
New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedUnit(newUnit)
Parameters: newUnit ( NXOpen.CAM.BoundaryTurnSetFeedUnitTypes
) –New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
FeedValue¶
-
BoundaryTurnVariableStockSet.
FeedValue
¶ Returns or sets the feed rate value
-------------------------------------
Getter Method
Signature
FeedValue()
Returns: Return type: float New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedValue(newValue)
Parameters: newValue (float) – New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
PositionFromStart¶
-
BoundaryTurnVariableStockSet.
PositionFromStart
¶ Returns or sets the position from start
-------------------------------------
Getter Method
Signature
PositionFromStart()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositionFromStart(positionFromStart)
Parameters: positionFromStart (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)