BoundaryTurnSet Class¶
-
class
NXOpen.CAM.
BoundaryTurnSet
¶ Bases:
NXOpen.CAM.BoundarySet
Represents a boundary turning set.
To create a new instance of this class, use
NXOpen.CAM.Boundary.CreateBoundaryTurnSet()
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
BoundaryMemberList | Returns the boundary member list |
BoundaryType | Returns or sets the boundary type |
CustomOffset | Returns or sets the flag whether this boundary has custom offset activated |
CustomStock | Returns or sets the flag whether this boundary has custom stock activated |
FeedUnit | Returns or sets the feed rate unit |
FeedValue | Returns or sets the feed rate value |
IgnoreFineFinishOffset | Returns or sets the ignore fine finish offset status |
Offset | Returns or sets the offset value |
OffsetIntent | Returns or sets the offset intent |
Plane | Returns or sets the boundary plane |
PlaneType | Returns or sets the boundary plane type |
PointList | Returns the points list |
Stock | Returns or sets the stock value |
Tag | Returns the Tag for this object. |
ToolPosition | Returns or sets the tool position |
ToolSide | Returns or sets the tool side |
Methods¶
Method | Description |
---|---|
AppendCurves | Add curves to the boundary |
CreateBoundaryMemberSet | Create an empty boundary member set @return |
RemoveCurves | Remove curves from the boundary |
Enumerations¶
BoundaryTurnSetFeedUnitTypes Enumeration | the types available for the feed rate unit |
Property Detail¶
CustomStock¶
-
BoundaryTurnSet.
CustomStock
¶ Returns or sets the flag whether this boundary has custom stock activated
-------------------------------------
Getter Method
Signature
CustomStock()
Returns: Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
CustomStock(newValue)
Parameters: newValue (bool) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
FeedUnit¶
-
BoundaryTurnSet.
FeedUnit
¶ Returns or sets the feed rate unit
-------------------------------------
Getter Method
Signature
FeedUnit()
Returns: Return type: NXOpen.CAM.BoundaryTurnSetFeedUnitTypes
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedUnit(newUnit)
Parameters: newUnit ( NXOpen.CAM.BoundaryTurnSetFeedUnitTypes
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
FeedValue¶
-
BoundaryTurnSet.
FeedValue
¶ Returns or sets the feed rate value
-------------------------------------
Getter Method
Signature
FeedValue()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedValue(newValue)
Parameters: newValue (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
IgnoreFineFinishOffset¶
-
BoundaryTurnSet.
IgnoreFineFinishOffset
¶ Returns or sets the ignore fine finish offset status
-------------------------------------
Getter Method
Signature
IgnoreFineFinishOffset()
Returns: Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
IgnoreFineFinishOffset(newValue)
Parameters: newValue (bool) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Stock¶
-
BoundaryTurnSet.
Stock
¶ Returns or sets the stock value
-------------------------------------
Getter Method
Signature
Stock()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Stock(newValue)
Parameters: newValue (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)