BoundaryTurnMemberFineFinishCorner Class

class NXOpen.CAM.BoundaryTurnMemberFineFinishCorner

Bases: NXOpen.Builder

Represents a NXOpen.CAM.BoundaryTurnMemberFineFinishCorner

This builder cannot be instantiated separately.

New in version NX9.0.2.

Properties

Property Description
AngleValue Returns or sets the fine_finish_corner angle value
AppliedToType Returns or sets the fine_finish_corner applied to
CleanupType Returns or sets the fine_finish_corner cleanup
Distance Returns or sets the fine_finish_corner distance
Tag Returns the Tag for this object.
Type Returns or sets the fine_finish_corner type

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

AngleValue

BoundaryTurnMemberFineFinishCorner.AngleValue

Returns or sets the fine_finish_corner angle value

-------------------------------------

Getter Method

Signature AngleValue()

Returns:
Return type:float

New in version NX9.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature AngleValue(cornerAngle)

Parameters:cornerAngle (float) –

New in version NX9.0.2.

License requirements: cam_base (“CAM BASE”)

AppliedToType

BoundaryTurnMemberFineFinishCorner.AppliedToType

Returns or sets the fine_finish_corner applied to

-------------------------------------

Getter Method

Signature AppliedToType()

Returns:
Return type:NXOpen.CAM.BoundaryTurnMemberFineFinishCornerAppliedTo

New in version NX9.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature AppliedToType(appliedTo)

Parameters:appliedTo (NXOpen.CAM.BoundaryTurnMemberFineFinishCornerAppliedTo) –

New in version NX9.0.2.

License requirements: cam_base (“CAM BASE”)

CleanupType

BoundaryTurnMemberFineFinishCorner.CleanupType

Returns or sets the fine_finish_corner cleanup

-------------------------------------

Getter Method

Signature CleanupType()

Returns:
Return type:NXOpen.CAM.BoundaryTurnMemberFineFinishCornerCleanup

New in version NX9.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature CleanupType(cornerCleanup)

Parameters:cornerCleanup (NXOpen.CAM.BoundaryTurnMemberFineFinishCornerCleanup) –

New in version NX9.0.2.

License requirements: cam_base (“CAM BASE”)

Distance

BoundaryTurnMemberFineFinishCorner.Distance

Returns or sets the fine_finish_corner distance

-------------------------------------

Getter Method

Signature Distance()

Returns:
Return type:float

New in version NX9.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature Distance(distance)

Parameters:distance (float) –

New in version NX9.0.2.

License requirements: cam_base (“CAM BASE”)

Type

BoundaryTurnMemberFineFinishCorner.Type

Returns or sets the fine_finish_corner type

-------------------------------------

Getter Method

Signature Type()

Returns:
Return type:NXOpen.CAM.BoundaryTurnMemberFineFinishCornerValueType

New in version NX9.0.2.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(cornerType)

Parameters:cornerType (NXOpen.CAM.BoundaryTurnMemberFineFinishCornerValueType) –

New in version NX9.0.2.

License requirements: cam_base (“CAM BASE”)

Method Detail

Validate

BoundaryTurnMemberFineFinishCorner.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.