BoundarySetToolSideTypes Enumeration

NXOpen.CAM.BoundarySet.ToolSideTypes is an alias for NXOpen.CAM.BoundarySetToolSideTypes

class NXOpen.CAM.BoundarySetToolSideTypes

Bases: object

the tool side types

New in version NX9.0.0.

Enum Members

Enum Member Enum Member Description
InsideOrLeft
inside for closed boundary, or left side for open boundary
OutsideOrRight
outside for closed boundary, or right side for open boundary
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.