BoundarySetBoundaryTypes Enumeration

NXOpen.CAM.BoundarySet.BoundaryTypes is an alias for NXOpen.CAM.BoundarySetBoundaryTypes

class NXOpen.CAM.BoundarySetBoundaryTypes

Bases: object

the boundary types

New in version NX9.0.0.

Enum Members

Enum Member Enum Member Description
Closed
close boundary
Open
open boundary
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.