BlankIpw Class¶
-
class
NXOpen.CAM.
BlankIpw
¶ Bases:
NXOpen.TaggedObject
Represents the blank ipw builder for blank definition
To obtain an instance of this class use the
NXOpen.CAM.GeometryGroup
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
GetSource | Get the blank ipw source @return the blank IPW source |
GetStatus | Get the blank IPW status @return the blank ipw status |
IsValidSource | Decide if the input object can be a valid source @return indicate if the input object is valid or not |
SetSource | Set the blank ipw source |
Update | Update the blank ipw @return the blank ipw status |
Enumerations¶
BlankIpwStatusTypes Enumeration | the blank IPW status types |
Method Detail¶
GetSource¶
-
BlankIpw.
GetSource
¶ Get the blank ipw source
Signature
GetSource()
Returns: a tuple Return type: A tuple consisting of (source, sourcePart). source is a NXOpen.CAM.CAMObject
. the blank IPW source sourcePart is aNXOpen.NXObject
. the part where the blank IPW source existsNew in version NX8.0.0.
License requirements: None.
GetStatus¶
-
BlankIpw.
GetStatus
¶ Get the blank IPW status
Signature
GetStatus()
Returns: the blank ipw status Return type: NXOpen.CAM.BlankIpwStatusTypes
New in version NX8.0.0.
License requirements: None.
IsValidSource¶
-
BlankIpw.
IsValidSource
¶ Decide if the input object can be a valid source
Signature
IsValidSource(object)
Parameters: object ( NXOpen.CAM.CAMObject
) – the object to be checkedReturns: indicate if the input object is valid or not Return type: bool New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
SetSource¶
-
BlankIpw.
SetSource
¶ Set the blank ipw source
Signature
SetSource(sourcePartName, sourceName)
Parameters: - sourcePartName (str) – the part name where the blank IPW source exists
- sourceName (str) – the name of the blank IPW source
New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Update¶
-
BlankIpw.
Update
¶ Update the blank ipw
Signature
Update()
Returns: the blank ipw status Return type: NXOpen.CAM.BlankIpwStatusTypes
New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)