BladeCutLevelsIncompleteLevelsTypes Enumeration

NXOpen.CAM.BladeCutLevels.IncompleteLevelsTypes is an alias for NXOpen.CAM.BladeCutLevelsIncompleteLevelsTypes

class NXOpen.CAM.BladeCutLevelsIncompleteLevelsTypes

Bases: object

Available types for Incomplete Levels

Enum Members

Enum Member Enum Member Description
OutputAndWarn
Output and Warn
Omit
Omit
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.