BladeCutLevelsDepthModeTypes Enumeration

NXOpen.CAM.BladeCutLevels.DepthModeTypes is an alias for NXOpen.CAM.BladeCutLevelsDepthModeTypes

class NXOpen.CAM.BladeCutLevelsDepthModeTypes

Bases: object

Available types for Depth Mode

Enum Members

Enum Member Enum Member Description
OffsetsFromHub
Offsets from Hub
OffsetsFromShroud
Offsets from Shroud
OffsetsAlongToolAxis
Offsets along Tool Axis
InterpolateFromShroudToHub
Interpolate from Shroud to Hub
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.