AreaMillingSteepContainmentCutLevelTypes Enumeration

NXOpen.CAM.AreaMillingSteepContainment.CutLevelTypes is an alias for NXOpen.CAM.AreaMillingSteepContainmentCutLevelTypes

class NXOpen.CAM.AreaMillingSteepContainmentCutLevelTypes

Bases: object

cut level types

New in version NX9.0.0.

Enum Members

Enum Member Enum Member Description
Constant
Constant
Optimized
Optimized
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.