AreaMillingNonSteepContainmentAmPocketDirTypes Enumeration

NXOpen.CAM.AreaMillingNonSteepContainment.AmPocketDirTypes is an alias for NXOpen.CAM.AreaMillingNonSteepContainmentAmPocketDirTypes

class NXOpen.CAM.AreaMillingNonSteepContainmentAmPocketDirTypes

Bases: object

Available types for Area Milling Pocketing Direction in FASurfaceContour

Enum Members

Enum Member Enum Member Description
Outward
Outward
Inward
Inward
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.