TextOrientation Enumeration

class NXOpen.CAE.Xyplot.TextOrientation

Bases: object

Represents the text orientation Enum Members

Enum Member Enum Member Description
Horizontal
Horizontal text orientation
Upward
Upward text orientation
Downward
Downward text orientation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.