PreferenceTargetGraphicWindowOption Enumeration

NXOpen.CAE.Xyplot.Preference.TargetGraphicWindowOption is an alias for NXOpen.CAE.Xyplot.PreferenceTargetGraphicWindowOption

class NXOpen.CAE.Xyplot.PreferenceTargetGraphicWindowOption

Bases: object

Defines the target graphic window type

Enum Members

Enum Member Enum Member Description
Main
Only shows plot graph on main graphic window
Separate
Only shows plot graph on a separate graphic window
Both
Shows plot graph on either main graphic window or a separate graphic window
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.