DecimalFormat Enumeration

class NXOpen.CAE.Xyplot.DecimalFormat

Bases: object

Represents the decimal number format Enum Members

for example: 5.3E+05 “
“Xxexx”, ” Scientific notation with two digits followed by period ” “Xxxexx”, ” Scientific notation with three digits followed by period ” “Xxxxexx”, ” Scientific notation with four digits followed by period “
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.