ContouringRange Enumeration¶
-
class
NXOpen.CAE.Xyplot.
ContouringRange
¶ Bases:
object
Represents the contouring range Enum Members
Enum Member Enum Member Description BorderGrid Option to show contour range on the border of the gridFullGrid Option to show contour range on the face of the grid-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-