ColorAxisStyleSetting Class¶
-
class
NXOpen.CAE.Xyplot.
ColorAxisStyleSetting
¶ Bases:
NXOpen.CAE.Xyplot.AxisStyleSetting
Represents the axis display style.
Call
CAE.Xyplot.IDisplayStyle.CommitChange()
to apply style changes to corresponding plot after it’s modified.Not support KF.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AxisType | Returns or sets the axis scale type |
ColorScaleStyleSetting | Returns the color scale display style. |
DbDecades | Returns or sets the number of dB decades to display. |
DbRef | Returns or sets the dB reference value for a dB axis type. |
DbScale | Returns or sets the dB scale. |
GraphOverhead | Returns or sets the round value to display. |
LogDecades | Returns or sets the number of Log decades to display. |
Owner | Returns the owner style |
Tag | Returns the Tag for this object. |
UnitSystem | Returns or sets the unit system |
UnknownResultScaleStyleSetting | Returns the unknown result scale display style. |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Find | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
Property Detail¶
ColorScaleStyleSetting¶
-
ColorAxisStyleSetting.
ColorScaleStyleSetting
¶ Returns the color scale display style.
-------------------------------------
Getter Method
Signature
ColorScaleStyleSetting()
Returns: Color scale style Return type: NXOpen.CAE.Xyplot.ColorScaleStyle
New in version NX11.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
Owner¶
-
ColorAxisStyleSetting.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner()
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.
UnknownResultScaleStyleSetting¶
-
ColorAxisStyleSetting.
UnknownResultScaleStyleSetting
¶ Returns the unknown result scale display style.
-------------------------------------
Getter Method
Signature
UnknownResultScaleStyleSetting()
Returns: Color scale style Return type: NXOpen.CAE.Xyplot.UnknownResultScaleStyle
New in version NX11.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)